FB#.SINGLETURNBITS

Description

Number of single turn bits used for BiSS rotary encoders. Feedback data sheet specifies the number required.

Context

Only used for when FB#.MECHTYPE is rotary and identified feedback is BiSS. See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

single turn bits

Range

1 to 32

Default Value

19
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
FB1.SINGLETURNBITS

3500h

0dh

Unsigned8

-

-

Read/Write

No

FB2.SINGLETURNBITS

3501h

0dh

Unsigned8

-

-

Read/Write

No

FB3.SINGLETURNBITS

3502h

0dh

Unsigned8

-

-

Read/Write

No

FB4.SINGLETURNBITS

3503h

0dh

Unsigned8

-

-

Read/Write

No

FB5.SINGLETURNBITS

3504h

0dh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.SINGLETURNBITS

30320

7670

Unsigned8

Read/Write

-

FB2.SINGLETURNBITS

30321

7671

Unsigned8

Read/Write

-

FB3.SINGLETURNBITS

30322

7672

Unsigned8

Read/Write

-

FB4.SINGLETURNBITS

30323

7673

Unsigned8

Read/Write

-

FB5.SINGLETURNBITS

30324

7674

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.SINGLETURNBITS

30320

Unsigned8

Read/Write

-

FB2.SINGLETURNBITS

30321

Unsigned8

Read/Write

-

FB3.SINGLETURNBITS

30322

Unsigned8

Read/Write

-

FB4.SINGLETURNBITS

30323

Unsigned8

Read/Write

-

FB5.SINGLETURNBITS

30324

Unsigned8

Read/Write

-